AXIS#.MT.MOVE

Description

This command needs one argument in order to start a motion task. The drive must be homed otherwise the motion task will not start.

Example

AXIS#.MT.MOVE 3 -> Start motion task number 3.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command Array

Units

N/A

Range

0 to 31

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MT.MOVE

6305

18A1

Unsigned8[32]

Read/Write

-

AXIS2.MT.MOVE

71841

118A

Unsigned8[32]

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.MOVE

6305

Unsigned8[32]

Read/Write

-

Related Topics

Motion Tasks